Post Go back to editing

adau7118

Category: Hardware
Product Number: ADAU7118

Hi Analog Devices Team,

I previously designed a PCB and successfully used one ADAU7118 chip to drive eight microphones for data collection. Now I want to expand to more microphones. I have designed a new PCB with two ADAU7118 chips that share the same I2C bus. I have soldered one chip along with its surrounding circuitry to test whether it can output a normal PDM_CLK signal (3.072 MHz), but I found that it cannot output a proper signal. Sometimes the I2C communication is correct but there is no PDM_CLK signal; other times the I2C communication works fine and the signal is correct for an instant before immediately going wrong. I don’t know if this is caused by a soldering issue or a problem with my circuit design. I will now upload screenshots of some of the signals. I really have no idea what is causing this problem.

Thank you.

Correct BCLK:

Correct FSYNC:

Correct PDM_CLK:

Incorrect PDM_CLK:

Parents
  • Hello, Dave

    I am using two separate TDM-8. My hardware configuration is as follows: the chip addresses are 0x14 and 0x15 respectively, register 0x05 is set to 0xC1, register 0x07 is set to 0x51, and all other registers remain unchanged. Each chip outputs its own sdata signal.

    Regarding the issue you mentioned where bclk is not an ideal square wave, I am not sure if this is caused by insufficient capability of my oscilloscope probes. I previously successfully designed a driver for 8 microphones using the ADAU7118 on my own, and I have not used the SigmaStudio tool yet, QAQ. I will now upload the PDF files of my hardware schematic and top-level design to you.I have another question: are there any points I should pay attention to when designing the PCB? For example, do BCLK and FSYNC need to be length-matched, or should I use as few vias as possible? I am quite worried whether this will affect the ADAU7118 and mic data, because my ultimate goal is to use 64 microphones.

    Additionally, I have found that the pdm_clk issue is resolved as long as I do not connect the sdata pin to the FPGA. I do not quite understand the principle behind this.

    Thank you.

    Hardware schematic:

    PDF

    PDF

    PDF of the top layer:

    PDF

  • Hello shandonguniversity,

    You are asking a lot of good questions and this opens up some deep and complicated topics. I will do my best to comment.

    I suggest you download the ADAU1452-Rev-D datasheet and look at the PCB Design considerations section. It is near the end of the datasheet. One of the things I talk about in that section of the datasheet is how to connect the EP. It is tough for me to see exactly what you have done but it looks like you connected it with a trace. I see a shadow on the PDF 

    Is this just a two layer board? 

    I strongly suggest you use at least four layers. It is not as expensive as it used to be many years ago... (I have been doing this for a long time!-LOL) 

    The bypass cap for the power is not placed and connected in such a way as to make it the most effective. C9 is the bypass cap.

    Again, in the ADAU1452 Rev D datasheet I show how these 0.1uf bypass caps need to be connected to make them the most effective. 

    I have seen this make a big difference. 

    I have seen problems customers have had that were caused by incorrect bypass caps and incorrect connections to the EP. 

    What is key here is to realize that a via is an inductor. Would you place an inductor between the power and the pin? Probably not. 

    Here is a link to the datasheet I mentioned above:

    ADAU1452/ADAU1451/ADAU1450 (Rev.D)

    Regarding the BCLK and LRCLK traces. Yes, it is good to have them be close to the same length but this does not have to be exact and is not a big cause of issues. Stray capacitance can be an issue and also return currents is also an issue. This is where having a single ground plane with few if any traces so it is a solid plane is important. The same goes for the power planes but often you end up having to split it because you have more than one voltage. Just think of the return currents. 

    Yes, use as few vias as possible when dealing with clocks and data. The inductance causes reflections and waveform problems. It is impossible to not have any!! So try to use a few as possible. 

    Additionally, I have found that the pdm_clk issue is resolved as long as I do not connect the sdata pin to the FPGA

    That is interesting!! What is the state of that pin on the FPGA? What is it set to? An input? Floating? This can add some stray capacitance and that would be my first guess but if it is set to be an input there might be internal pull-ups. Of course, if it is set to be an output would be bad!! 

    Since this account is from a school, I suggest looking into signal integrity concepts. This goes into the art form of PCB design. It certainly is an art form for sure and is very creative and I like that. It is a challenge at times!!

    Thanks!

    Dave T

Reply
  • Hello shandonguniversity,

    You are asking a lot of good questions and this opens up some deep and complicated topics. I will do my best to comment.

    I suggest you download the ADAU1452-Rev-D datasheet and look at the PCB Design considerations section. It is near the end of the datasheet. One of the things I talk about in that section of the datasheet is how to connect the EP. It is tough for me to see exactly what you have done but it looks like you connected it with a trace. I see a shadow on the PDF 

    Is this just a two layer board? 

    I strongly suggest you use at least four layers. It is not as expensive as it used to be many years ago... (I have been doing this for a long time!-LOL) 

    The bypass cap for the power is not placed and connected in such a way as to make it the most effective. C9 is the bypass cap.

    Again, in the ADAU1452 Rev D datasheet I show how these 0.1uf bypass caps need to be connected to make them the most effective. 

    I have seen this make a big difference. 

    I have seen problems customers have had that were caused by incorrect bypass caps and incorrect connections to the EP. 

    What is key here is to realize that a via is an inductor. Would you place an inductor between the power and the pin? Probably not. 

    Here is a link to the datasheet I mentioned above:

    ADAU1452/ADAU1451/ADAU1450 (Rev.D)

    Regarding the BCLK and LRCLK traces. Yes, it is good to have them be close to the same length but this does not have to be exact and is not a big cause of issues. Stray capacitance can be an issue and also return currents is also an issue. This is where having a single ground plane with few if any traces so it is a solid plane is important. The same goes for the power planes but often you end up having to split it because you have more than one voltage. Just think of the return currents. 

    Yes, use as few vias as possible when dealing with clocks and data. The inductance causes reflections and waveform problems. It is impossible to not have any!! So try to use a few as possible. 

    Additionally, I have found that the pdm_clk issue is resolved as long as I do not connect the sdata pin to the FPGA

    That is interesting!! What is the state of that pin on the FPGA? What is it set to? An input? Floating? This can add some stray capacitance and that would be my first guess but if it is set to be an input there might be internal pull-ups. Of course, if it is set to be an output would be bad!! 

    Since this account is from a school, I suggest looking into signal integrity concepts. This goes into the art form of PCB design. It certainly is an art form for sure and is very creative and I like that. It is a challenge at times!!

    Thanks!

    Dave T

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.