Post Go back to editing

ESD and accidental line-in protection

Thread Summary

The user inquires about ESD protection and safeguarding the MAX9728A headphone amplifier from accidental line-in insertion. For ESD protection, a TVS diode is recommended due to its fast response to voltage transients. To protect against line-in voltage, a low forward voltage diode clamp is suggested if the line-in voltage exceeds the absolute max ratings of 9V above SVSS or VDD + 0.3V, and 9V below VDD or SVSS - 0.3V.
AI Generated Content
Category: Hardware
Product Number: MAX9728A , MAX9728

Hello,

I am looking to use MAX9728A in a product for a headphone output.  I wanted to ask a couple of questions.

1.  What would you suggest for ESD protection near the external audio jack connection, for example a Zener diode?

2.  The audio headphone output jack is a standard 6.35mm or 3.5mm jack. The product i am working on has an audio line-in with a similar jack.  What protection can I use to protect against damage to the amplifier caused by users accidental insertion of the line-in (standard consumer voltage levels) to this headphone jack.  Would I need a low-forward voltage diode or similar, or would the amplifier be ok with the line-in voltage applied to the OUT_L and OUT_R pins?

Thanks for your help

  • Hello, thanks for the questions.

    Though I cannot give a specific recommendation for ESD mitigation for your application, I will point out that a common ESD mitigation technique is to use a TVS (transient voltage suppression) diode placed closely to the audio jack with a short path to ground. TVS diodes react more quickly to voltage transients than Zener diodes. This may prove effective for your situation.

    For your second question, the MAX9728A datasheet lists the absolute max rating for the OUTL and OUTR as described below (found on page 2 of datasheet):

    "Note 1: OUTR and OUTL should be limited to no more than 9V above SVSS, or above VDD + 0.3V, whichever limits first.

    Note 2: OUTR and OUTL should be limited to no more than 9V below VDD, or below SVSS - 0.3V, whichever limits first."

    If you find that an accidental insertion may exceed those limits, you could try a low forward voltage diode clamp. There are other mitigation techniques that may work, but this is a common one.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.