Post Go back to editing

Selecting the minimum R_IN value for the MAX97220A

Thread Summary

The user inquired about the minimum RIN value for the MAX97220A and whether using RF = 12kΩ and RIN = 1.9kΩ is feasible. The support engineer confirmed that there is no specific minimum RIN value for the MAX97220A and that the selected values should work, provided the CIN capacitor is chosen to achieve the desired input filter response as detailed in the MAX97220 datasheet.
AI Generated Content
Category: Hardware
Product Number: MAX97220A

What is the minimum RIN value when using the MAX97220A?

I want to use an RF of 12KΩ and the RIN of 1.9 KΩ. Is there any problem? Is it possible?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.