Hi ADI
Now I use MAX98357 , how to use MAX98357 adjust the volume ?
Thanks
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
MAX98357A
Production
For improved performance, functionality, and even lower power consumption Maxim Integrated recommends the MAX98360.
The MAX98357A/MAX98357B is an easy...
Datasheet
MAX98357A on Analog.com
Hi ADI
Now I use MAX98357 , how to use MAX98357 adjust the volume ?
Thanks
Hello TYW576,
I am going to jump in and respond to your question since our expert on this part, Mike, is on the west coast and I hope is still enjoying a good sleep! So he might correct me on this response but I think I got this.
This part does not have what I would call a volume control. A volume control like a pot where you can go from no audio to full volume of what is coming into the part or even add gain.
If you are using the part in I2S mode then you have the GAIN_SLOT pin which allows you to adjust the gain of the amp but this is not a volume control. Table 8 in the datasheet describes the settings.

If you are using TDM instead of I2S digital signal format, then this pin will select the slot that this part uses and the gain is fixed at 12dB.
So you need to implement your volume control in your DSP. What DSP are you using?
Thanks,
Dave T
Dave is correct, there. There is no volume controller, and it is not advised to change the gain during operation as it can result in click pop.
As already suggested, the best way to create a digital volume controller back at the DSP.
Hi Dave T
Thank you very much
Thank you , I use DSP reslove the problem