Post Go back to editing

Maximum output current on CM pin?

Category: Hardware
Product Number: ADAU1361

Hi everyone

I am actually using the CM pin of ADAU1361 as the negative input on a AOP differential amplifier.

The impedance seen from the CM pin is around 40 kohm. The CM pin is also connected to LIN_P input pin.

As a result, the CM voltage is not stable, around 1 to 1,4 V between different products, instead of 1,65V (AVdd/2).

Is the current consumption too much for that pin? Is the impedance of my AOP amplifier too low?

I did not find the answer on the forum...Sorry 

Thanks a lot!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.