I am looking at several of Analog's boosted Class-D amplifier offerings, including the MAX98380, MAX98390, and SSM4567. I will be running from a large, single-cell LiPo battery and I would like some objective and subjective opinions about which of these amps is the best. I will not be using any of the dynamic speaker management features of the MAX98390 and I'm not sure if this is the only difference between the '380 and the 390. Meanwhile, I assume that the MAX parts originated at Maxim and the SSM part is an Analog original.
This is a fairly low-power application, needing no more than 2.5W output, mono. The amplifier will be fed from I2S digital, not analog.
Edit Notes
[locked by: DaveThib at 1:57 PM (GMT -4) on 20 Aug 2024]