Hi,
SSM6515
Recommended for New Designs
The SSM6515 is a fully integrated, high efficiency, mono Class-D audio amplifier with digital input that is ideally suited for use in wireless headphones...
Datasheet
SSM6515 on Analog.com
Hi,
Hello gzav,
I will notify galvinpjg about your question. He is the applications engineer who knows this part the best.
Dave T
Gzav,
1) In mute mode, there will still be output pulses on the OUT+ and OUT- pins. The modulator is still generating pulses and these are present at the output stage. The modulator is still active.
1b) Setting DAC_MUTE will be have the same as above, as will setting DAC_VOL to 0xFF. The only difference is that DAC_MUTE may be faster or slower depending on SOFT_MUTE being enabled or disabled.
2) In shutdown mode, the output stage is hi-z relative to the outputs. The outputs are not driven.
Thank you