Post Go back to editing

DSP Core is SLEEP mode after loading program.

Category: Datasheet/Specs
Product Number: ADAU1462

Hello,

I'm having a slight issue with the ADAU1462 DSP. I have a custom designed board that uses the DSP, and am loading software onto the board via SPI external microcontroller.

My issue is that after loading a simple S/PDIF IN to Serial Audio Out program from Sigma Studio, the core status register (0xF405) is reading 0x0011 which according to the datasheet corresponds to "core sleeping".

From what I gather in the datasheet, if the core is not killed, not hibernating, and started, the only way it would sleep is if the program issues a sleep instruction, OR if there is a PANIC flag somewhere.

All panic flags are enabled, but the panic register is showing 0 (no panic). This leads me to believe that somehow my SigmaStudio program is causing the core to sleep, but I'm not sure why it would do this.

I have previously successfully programming an ADAU1701 with the same method, again using SigmaStudio, and it has worked perfectly each time.

Thank You,