Post Go back to editing

Input and output characteristics

Category: Datasheet/Specs
Product Number: MAX98089

Hello,

I'm considering the MAX98089 for a project and I have several questions regarding the input/output characteristics.

  • Input: my intention is to use the microphone input although the signal doesn't come from a microphone. This is because I need to use the AGC and the line input doesn't have it, and because the input impedance for microphone line is constant (not for line input which impedance is dependent on applied gain). 
    • What is the input voltage for full scale? According to page 7 of datasheet it is 1.05Vpp when AVmicpre=0dB, but does it need any DC offset? According to absolute maximum ratings, mic input voltage goes from -0.3V to +2.2V. Does it mean I have to sum a DC offset to my input signal of... 1V for example? Can this reference be taken from MICBIAS to implement a simple sum with an OPAMP?
  • Output: my intention is to connect an amplifier to the speaker output (or maybe a transformer coupled load, it depends on the information I need) 
    • What is the output voltage for full scale? I mean with no load. According to page 15 on datasheet it is 2Vrms, but I suppose it depends on Vspkvdd. Also if you calculate the output voltage for spk based on power data it is 3.05Vrms for 4ohm 1% THD. (I supposed power data is RMS, is it right or is it peak?)
    • I suppose the output for spk doesn't have any DC offset and doesn't need any AC copling.
    • What is the output impedance? Based on output power data I obtained that output impedance (on diff mode) is 0.72 ohm. Is it right?

Thanks in advance.

Parents
  • Input:

    • On the bench, I was able to reach full-scale speaker output voltage with up to 1.44 Vp-p on the input.  This is higher than what the datasheet reports, so I would still recommend not exceeding the 1.05Vp-p to ensure that that the input will not clip.
    • The input signal that I used was single-ended referenced to ground, but it uses a 1µF AC coupling capacitor in series with the MIC1 P input.  MIC1 N was tied to ground, also with a 1µF capacitor in series.

    Output:

    • Without a load, the output can approach ~2x Vspkvdd without exceeding 1% THD.
      • Vspkvdd = 5.5V (EC Table Maximum)
      • MIC1 input = 1.022Vpp
      • MIC1 gain = 0dB preamp, 0dB PGA
      • Speaker gain = 6dB
      • Speaker Output = 3.855Vrms (10.9Vp-p) @ 1% THD+N

    Attached is a scope shot of the speaker output with 1% THD+N.  The output is starting to clip on the positive edge as it is reaching the limits with such a large signal.  The scope shot includes the speaker outputs before and after going through a low-pass filter.

    MAX98089 Speaker Output

    I am still researching the output impedance.  I will update this if I am able to locate this data.

  • Hello Ed,

    First of all thank you so much for your help, it will be very useful for me.

    I have some question:

    • Input: regarding the input you said that it is recommended not to surpass 1.05Vp-p (0.5Vp). As you used decoupling capacitors the input signal is AC only with MICP= +0.25Vp and MICN=-0.25Vp. This allow not exceeding the -0.3 to +2.2V range indicated in the absolute maximum ratings but is really near the minimum value and quite far of the maximum value. Is it not really needed a DC offset and dc coupling at the input? (I mean, no capacitors in series).
    • Output: Is it possible to see a scope shot of the headphones output with no load under the same testing conditions? With 0dB gain at the output I mean, as the headphones doesn't have the 6dB amplifier.

    If you know the output impedance for speaker stage and headphones stage please let me know.

    Thank you very much.

  • Hello, Agarciagon,

    I am using the MAX98089 EVKit to make the bench measurements.  Please find the schematic at the following link: max98089evkit_wlp.pdf (analog.com)

    I am applying the input signal to the MIC1P test point, which passes through the 1µF AC coupling capacitor C121.  I have JU36 inserted, which applies ground to the input side of C118 which AC couples the MIC1N pin.

    The input signal that I'm using is 1Vp-p, single-ended referenced to ground, so the input is a 0V - 1V signal.

    If you do not want to use coupling capacitors at the input, be aware that the signal needs to be biased at ~AVDD/2.  If the bias is not set correctly on the input signal, there will be DC components on the output signal.  It is much easier to use capacitors in series to prevent this.

    Here is a screenshot of the headphone output, unloaded, with a 1Vp-p input on MIC1P and with the headphone gain set to 0dB.

    I am still researching the output impedance.

  • Hello Ed,

    Thank you very much for the information. About the filtered class D signal you showed, is it taken after the filter it is present in the evaluation board?

    II mean this one:

    Thank you,

  • Hello, agarciagon,

    My filtered scope shot was taken after the signal passed through an Audio Precision AUX-0025 Class D Filter.

    The filter on the EVKit is intended to reduce EMI when using long speaker cables.  I don't think that it is sufficient to remove all of the high frequency switching from the speaker outputs if that is a requirement for the amplifier that will be connected to it.

Reply
  • Hello, agarciagon,

    My filtered scope shot was taken after the signal passed through an Audio Precision AUX-0025 Class D Filter.

    The filter on the EVKit is intended to reduce EMI when using long speaker cables.  I don't think that it is sufficient to remove all of the high frequency switching from the speaker outputs if that is a requirement for the amplifier that will be connected to it.

Children
  • Hello Ed,

    Thank you for your response. Another doubt that comes to me is regarding the mic to adc frequency response graph that is located on page 29 on the datasheet.

    First of all, I suppose this is the characteristic behaviour of the codec from the input to the ADC, without taking into account digital voice filters after the ADC.

    Where it is specified 'freq mode' I suppose it means that clocking mode is working on Exact Integer Mode (table 11 register 0x11), and the two indications of "MODE=1" and "MODE=0" I suppose it refers to IIR and FIR. But I'm not pretty sure because I've readen that there is a 'MODE1' parameter in register 0x18 that configurates the passband filtering mode, but this passband filter is located after the ADC. And I've not seen any "MODE" parameter in the registers. Moreover, in page 7 it says that MODE=0 is IIR voice and MODE=1 is FIR audio.

    Can I get your help to clarify this?

    Thank you.