Post Go back to editing

SSM2019 and PKGS-00GXP1-R

Category: Hardware
Product Number: SSM2019

I would like to use the low noise SSM2019 in combination with the to surface mountable piezo acceleration sensor PKGS-00GXP1-R.

The piezo sensor is 390pF >500MOhm and generates 35.7 fC/(m/s^2)

Bandwith should be between 5 and 500Hz.

Typically an acceleration sensor can be interfaced with a charge amplifier (low impedance) or voltage amplifier (Q=C*V) high impedance.

I am not sure how the SSM2019 input impedance can be assessed.

Any advice is welcome.