Post Go back to editing

How does the shutdown feature for MAX9722A work?

Category: Hardware
Product Number: MAX9722A

How does the shutdown feature for MAX9722A work?

I'm currently testing MAX9722A with a setup similar to the typical application circuit given in the data sheet w. 6dB gain configured by external resistors.

However, when I pull the shutdown pin low and load the output with a 250 Ohm headset, the input is still very much hearable. I understand that the shutdown pin is not a mute feature, but according to the oscilloscope images in the data sheet, the output should be ~0V when the shutdown pin is held low.

  • Thank you for your interest in the MAX9722A.  I've reviewed the conditions and had a few basic checks done in the lab. Placing the MAX9722A in SHDN will allow for low current consumption and place the outputs in high-impedance mode (10kΩ).  As you surmised, there is no active mute and that is not possible since there are external resistors to the MAX9722A.  As a result, there is an external pathway for some amount of signal to pass from the input to the output.  There should be significant attenuation on this of at least 60dB.  However, that may not be enough to completely mute a headphone set.  While in SHDN, RF+RG act as a resistor with the output load. You should be able to increase the output attenuation by increasing RF & RG while keeping the desired gain.

    The best solution would be to disable the input signal when placing the MAX9722A in SHDN mode.

  • Hi Mike,

    Thanks for testing this for me.

    Yes, I figured it might have been "leaking" through the gain setting resistors.
    My solution will be to disable the input whenever the SHDN pin is set low as you suggested.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.