The customer is conducting an operation test and is having difficulty setting up the initialization via I2C. Are there any example codes or SW Guide materials related to MAX20317 I2C?
MAX20317
Production
The MAX20317 is an I2C controllable, universal 3.5mmØ accessory management IC. The device provides a universal jack interface solution, as well as a compact...
Datasheet
MAX20317 on Analog.com
hello
Is it impossible to provide what I requested?
Hello anthony81,
Sorry we let this request slip by without an answer.
I assume at this point there are no further questions. If there still is it would be good to include a lot more detail in your post. Provide the initialization procedure that is not working correctly. Give us something to work with rather than "it is not working".
What operation was not working? What was this test being performed?
That will help us get to an answer much more quickly.
Thanks,
Dave T