We have an 8 channel audio capture design using two ADAU1772. Eight external microphone inputs are amplified and provided to CH1-4 of each of the two CODECs. Two of the four channels on CODEC2 can be configured to utilize external mics or internal DMICs (TDK T5837). Encoded data is transmitted via TDM8 to the MCU. External microphone channels are nice, clean and properly leveled, but the DMIC audio is extremely low (~40dB below mic channels). Is it required to run those DMIC channels to the DSP of the ADAU1772 and provide a gain stage similar to what would be required for an analog microphone?
Thank you, Robert S.