Hello to every one, I hope you doing well.
I need some help about AD1937 datasheet. While reading the datasheet of this IC, I came across common-mode voltage topic and now I need your help to understand it better. Common mode voltage is discussed on page 15 of the IC 1937 datasheet. What is the purpose of this voltage? Should our input signal have a common mode voltage? Is it necessary that our input voltage has DC offset? In the following, it is mentioned that this voltage can be used to bias external op-amps, and as mentioned, this voltage is around 1.5 volts. Does the data sheet mean that we can use this voltage to bias vcc of op amps with this voltage? I think this voltage is a little low to bias the op amp. In the parameter table of this IC, it is written that the input signal of this IC can be 2.05 V RMS, in other words, its peak voltage can be 3 V. Now is this 3 volts considering ground as crossing zero? Or the zero crossing point of our signal will be considered 1.5 volts and our peak voltage can increase to 4.5 volts?
Thanks for your helps.