Hi,
I've been looking into audio ADC's and based on my research do I think that the ADAU1978 works for my application.
I was wondering if it is possible to do internal oversampling inside the chip. I want to sample at 192kHz but output the data at 48kHz.
I did see that there are multiple settings to set the sampling frequencies, but it is not clear to me if the above mentioned oversampling is possible.
Also do I want to know how the characteristic of the digital filter looks like at 192kHz since the digital filter in the datasheet is based on 48kHz.
Look forward to a response.
Tom