Post Go back to editing

Interfacing MAX9744 with Audio Codec

Thread Summary

The user inquires about using the MAX9880A to interface with the MAX9744 for stereo audio output. The support engineer suggests using the MAX9860 or MAX9867 headphone CODECs, which have single-ended outputs compatible with the MAX9744. Alternatively, the MAX98365 mono speaker amps are recommended for a simpler solution.
AI Generated Content
Category: Hardware
Product Number: MAX9744

Hi,

We are using MAX9744 to provide Stereo audio output for 2 speaker with 5W power for each. On MCU side we have the I2S and therefore we need to use the Audio CODEC with I2S. For MAX9744 the audio input pins are INL and INR so is there any Audio Codec that we can use to interface with MAX9744?

Please confirm if we can use MAX9880A with its LOUTR and LOUTL connected to the MAX9744 INR and INL pins. We are OK to do so but there are many other interfaces on MAX9880A that are useless for our application. If there is any other suitable CODEC for MAX9744 then please suggest. 

Kind regards,

Muhammad Awais