SSM3582
Not Recommended for New Designs
The SSM3582 is a fully integrated, high efficiency, digital input stereo Class-D audio amplifier. It can operate from a single supply, and requires only...
Datasheet
SSM3582 on Analog.com
Dear Team,
We are using the following Amplifier : Class D SSM3582

We would like to know how much is the delay between Amp In -> Amp Out for this Class D Amplifier .
Also how much is the latency generally (a range would be helpful, min,max) between Amplifier In and Amplifier Out for a Class D Amplifier .
Also what other factors in the hardware can possibly contribute to a significant delay such as RCA cables used for Amplifier Input , AWG Speaker wires used to connect to Speaker Output, length of wires , speed of signal etc .
Regards,
Hermione
PaulCA - Moved from Differential Amplifiers to Audio. Post date updated from Thursday, November 30, 2023 to Friday, December 1, 2023 to reflect the move.
PaulCA - Moved from Differential Amplifiers to Audio. Post date updated from Friday, December 1, 2023 to Friday, December 1, 2023 to reflect the move.
Hello ,
I have moved this query to the Audio Community. Someone there should be able to assist you better.
Best regards,
Paul
Hermione,
The latency for SSM3582 is approx. 15uS at 192kHz, 30uS at 96kHz and 60uS at 48kHz. For the amplifier, the main variable is the sample rate, increasing the rate can reduce latency. The only other external factor in our measurements that needs to be accounted for is the 5.7uS latency in the AUX-0025 switching amplifier filter.
Thanks galvinpjg,
What I forgot to ask earlier in my post is what would be the expected delay from Amplifier In to Amplifier Output for a 20kHz Input Signal assuming 48kHz Sample rate?
Also do Input Signal Frequency influence delay for a fixed sample rate of 48kHz?
Also I was wondering if you would mind sharing with me the procedure to measure this delay so that I can run this test in my lab .
Regards,
Hermione
Dear Team,
Its been a while since I heard from you. Can you please provide insights to my queries above.
Regards,
Hermione
Please support in this.
Regards,
Hermione
Hi Hermione, I have reached out to the product applications engineer. Thank you for your patience here.
Dear emassa,
Thank you so much for your support.
Looking forward to any response from the engineer side.
Regards,
Hermione
Hello Hermoine,
Patrick did answer your questions. The delay is mostly due to the sampling rate. Any IIR or analog filters will also create a phase shift and add some latency based on frequency of the audio. Any FIR filters will just add a fixed latency for all frequencies. So your total latency will depend s little on your processing.
Notice the numbers from Patrick. At 48kHz it was 60us. The switching amplifier filter that is used to filter out the out of band noise is an analog filter and you see it adds another 5.7us of latency.
So depending on your processing there may be a small change in latency based on signal input frequency but it usually is not a lot. If you were running at 192kHz fs then it can become more significant.
As far as a procedure to share. Our procedure is simple with the test equipment we have. We use the Audio Precision APx system. We have the serial digital output option and the analog input option. We go out of the digital serial port directly into the amp using I2S. Then the output of the amp goes to the switching filter and the filter output goes into the analog input of the Audio Precision. Then we setup the test equipment to use the correct inputs and outputs and you can then measure the latency. It will read it on the computer screen for you. It is very easy.
If you do not have that then it is a little more difficult. You would need to use an oscilloscope and the best signal to use is a tone burst. This way you will know you are not one or more full wavelengths off. Then measure the time on the scope.
I hope this helps.
Dave T