Post Go back to editing

MAX9792 input levels

Category: Hardware
Product Number: MAX9792

I'm designing a portable/mobile circuit using MAX97292 to amplify the output of a DAC.

I need to keep the circuit the more compact as possible (this's one of the reason I'm using MAX9792 because it doesn't need large output filters its outputs).

I would also like avoid using active components between DAC and MAX9792 inputs if possibile.

DAC application note prescribe to put some high frequency filters and a DC blocking capacitor on its outputs. MAX9792 require an RC filter on its inputs (DC blocking caps).

I would like to undestand if such a passive network will fit the needs and if input levels are matching MAX9792 needs. So I decided to run a simulation (AC sweep between 20Hz to 20KHz).

This's the simulated circuit:

Of course V1 and V2 are the outputs of the DAC while the opamps on the left side are a simulation of the internal network of MAX9792.

The resulting simulated output is something like that:

I think is coeherent since all MAX9792 inputs (SPKR_In, HP_INL, HP_INR) all levels  on -3.6dB (half the input level?).

To achieve such levels I needed to replace the recommended 40.2k resistors on HP_INL and HP_INR lines and put 20k resitors (like those on SPKR_IN)... is this correct?

Since caps prescribed for SPKR_IN, HP_INL, HP_INR inputs are required for the same purpose of those on DAC output is possibile to remove them?

They are fairly lower than those on DAC output...

Edit Notes

moved and tagged
[edited by: GenevaCooper at 2:08 PM (GMT -5) on 20 Nov 2023]

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.