Post Go back to editing

Possible to use MAX5440 with log potentiometer to control the attenuation taps?

Product Number: MAX5440

Hello, I want to use MAX5440 as a voltage control with a logarithmic 25k potentiometer. Log pot in its furthest position should put MAX5440 to max -90 dB attenuation (tap 32). If I leave both rotary inputs of MAX5440 open, W0/W1 open, connect my L/H inputs to terminals of the pot, would this solution work?

Edit Notes

non e
[edited by: GRPEE34 at 3:11 PM (GMT -4) on 28 Sep 2023]
Parents Reply Children
No Data