Post Go back to editing

MAX98089 THD+N performance

Category: Datasheet/Specs
Product Number: MAX98089 THD+N measurment


Hi Support team,

MAX98089 datasheet shown the THD+N can support around -80dB for all audio band, we are trying to test it from EVK and provide 48K audio from the AP.

But we cannot get the THD+N under -80dB as well, could you help to review the file and give some suggestion to improve THD+N performance? 


 DOCX

  • Hello, JustinWu_Ans,

    When the performance is so much worse than what the MAX98089 is supposed to deliver, there is usually something misconfigured or there is a problem with the I2S DAC inputs.

    I have just quickly checked the performance of my MAX98089 EVKit compared to the datasheet TOC plot in the middle of page 47, and while my plots are not identical, they are closer than what you are seeing.  My test cables and loads are not optimal, so this performance could be improved.

    The first place that I would look for problems would be the I2S signals.  Ensure that they are using the same voltage level as VDVDDS1 and VDVDDS2.  The part may appear to function when the I2S signals don't match the S1S2 voltages, but the performance will be degraded.

    Also make sure that the DAI input is formatted correctly.  If you are using I2S delay or not, make sure that the MAX98089 is configured properly.  A mismatch in this configuration will also cause poor performance.

    If you can capture an FFT of the HP outputs, it might provide more clues as to what is causing the poor performance.

    If you are able to attach a control register data dump to a reply, I can look it over and see if there is anything that stands out to me as being misconfigured.

  • Hi EdSeller,

    thanks for your advise , i will check with customer for details. 

    please find our setting as attached , if you have any comment , please kindly let me know.

    SPDIF_USB_Analog_Mixer to analog+USB_route to SPDIF_output_FINAL_20230919.zip

    BR

    thanks for your help.

  • Hi Edseller,

    we have confirmed the audio interface , we are using the Left-Justified , since the test is by MAX98089_EVB , we also check the voltage between VDVDDS1 and VDVDDS2 was same level. 
    but we use external digital audio source to the DAI1.

    BTW , I just find the setting for the DAI1 is left-justified and DAI2 is I2S , do you think it will cause some problem here? 

    BR

    Justin

  • Hello, Justin,

    As long as the data source for each DAI matches how the MAX98090 is configured, there will not be any problem.  They can function independently of one another.