Post Go back to editing

ADAU1978-PLL/Clock for fs = 16kHz, any kind of simulation model available

Category: Software
Product Number: ADAU1978

ADAU1978:

The datasheet did not show how to configure the PLL/Clock for a 16kHz sampling frequency.

Rev. A | Page 13 of 44: It seems only sampling frequencies 32kHz and above are supported? Also Table 9 did not show settings for fs = 16kHz.

In Table 1 fs is specified from 8 kHz to 192kHz.

Question: How must be the PLL/Clock configured for fs = 16kHz?

Is there a simulation model available (VHDL, Spice, MATLAB, …)?

Parents
  • Kfraus,

    Please see the table below.  16kHz is indeed supported, so long as the PLL is in MCLK mode.  The 32kHz restriction is applicable if the PLL is in LRCLK Mode.  But MCLK mode for PLL should work with 16kHz.  

    If FS = 16kHz, then the FS bits should be set to b001.  From there, the MCS bits will be set accoridng to the frequency of MCLK.  If MCLK = 8.192MHz for example, then MCLK:LRCLK ratio = 512.  Hence the MCS bits should be set for "512" in the "16-24kHz" row of the table.  This means MCS bits = b001.

    FS: Bits [2:0] of Register Address 0x05 MCS: Bits [2:0] of Register Address 0x01
    000 001 010 011 100
    MCLK:LRCLK Ratio
    [000] /  8 - 12 kHz 512 1024 1536 2048 3072
    [001] / 16- 24 kHz 256 512 768 1024 1536
    [010] / 32- 48 kHz 128 256 384 512 768
    [011] / 64 - 96 kHz 64 128 192 256 384
    [100] / 128 - 192 kHz 32 64 96 128 192
    Note:  This table assumes a minimum of 2 channels.

    Please let us know if there are additional questions.

    Thanks,
    PG

Reply
  • Kfraus,

    Please see the table below.  16kHz is indeed supported, so long as the PLL is in MCLK mode.  The 32kHz restriction is applicable if the PLL is in LRCLK Mode.  But MCLK mode for PLL should work with 16kHz.  

    If FS = 16kHz, then the FS bits should be set to b001.  From there, the MCS bits will be set accoridng to the frequency of MCLK.  If MCLK = 8.192MHz for example, then MCLK:LRCLK ratio = 512.  Hence the MCS bits should be set for "512" in the "16-24kHz" row of the table.  This means MCS bits = b001.

    FS: Bits [2:0] of Register Address 0x05 MCS: Bits [2:0] of Register Address 0x01
    000 001 010 011 100
    MCLK:LRCLK Ratio
    [000] /  8 - 12 kHz 512 1024 1536 2048 3072
    [001] / 16- 24 kHz 256 512 768 1024 1536
    [010] / 32- 48 kHz 128 256 384 512 768
    [011] / 64 - 96 kHz 64 128 192 256 384
    [100] / 128 - 192 kHz 32 64 96 128 192
    Note:  This table assumes a minimum of 2 channels.

    Please let us know if there are additional questions.

    Thanks,
    PG

Children
No Data