Post Go back to editing

SigmaStudio, ADAU1701 and Windows 11 on M2 Mac running Parallels

Category: Hardware
Product Number: ADAU1701
Software Version: SigmaStudio 4.7

Hey all,

I'm running a MacBook Pro M2 with Windows 11 on Parallels and am running SigmaStudio just fine. I am running into a problem with the included programmer for the EVAL-ADAU1701MINIZ (https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADAU1701.html).

The USBi programmer (EVAL-ADUSB2EBZ) is showing up under Other devices in device manager and what I've found in looking through other documentation is the following:

"Connect the USBi to an available USB 2.0 port using the USB cable included in the evaluation board kit. (The USBi does not function properly with a USB 3.0 port.)"

That quote is from this documentation for another eval kit that uses the same programmer: https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADAU1777Z-UG-1055.pdf

I can't tell if it's because I'm on an ARM processor now and there are no ARM drivers for this programmer or if the issue is actually USB 3, in which case... that's all I have on my computer. I tried a USB hub to try and see if it would recognize it as a USB 2.0 device but that didn't seem to do anything. I tried adding the drivers manually but it says it can't find the drivers when I point the manual driver folder to the Sigma Studio driver folder.

So my question is... is there anyway to get this to work with Windows 11 or USB 3? I know the Parallels thing and the ARM processor changes things.

Or, is there another programmer I can buy that will still work with the ADAU1701 eval board?

Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.