Post Go back to editing

ADAU1462/66 S/PDIF RCA Input

Product Number: ADAU1462

Hello,

For a digital amplifier design I need a RCA S/PDIF input and output on a ADAU1462 (192kHz max). I want a transformer on the input and was thinking of some design similar to this (maybe with a SN65LVDM176 instead of the MAX3280):

 

Can someone confirm that this would work? Or is there a simpler/better/cheaper solution? How about the grounding of the RCA shield, should this be PE or could it be floating ? I am a bit concerned about ground loops.
Also what kind of circuit would I need on the TX output of the ADAU for the S/PDIF thru ? It seems like the output signal is 3V3 p-p, so i assume I need a level conversion back to the 0.5V p-p to comply with the level standard for S/PDIF.

Thanks in advance, 

Best, 
Max

Parents
  • Hello Max,

    If you do not mind, I will refer you over to one of the best places for digital transformers and information. Look at the published papers on the web site. It has super detailed analysis. 

    In my opinion you should nt have to ground the input. The transformer primary will see the difference of the signal to the remote ground so you do not and should not ground it locally. It is somewhat the point of using a transformer. 

    Using a good differential input amp will be the best for good CMRR. You may not HAVE to do this, you could ground the secondary and then drive our input stage in the DSP. It would need to be cap coupled. However, read these articles and see what would be best for your application. 

    Scientific Conversion, Inc. - Transformers and Inductors (scientificonversion.com)

    Dave T

Reply
  • Hello Max,

    If you do not mind, I will refer you over to one of the best places for digital transformers and information. Look at the published papers on the web site. It has super detailed analysis. 

    In my opinion you should nt have to ground the input. The transformer primary will see the difference of the signal to the remote ground so you do not and should not ground it locally. It is somewhat the point of using a transformer. 

    Using a good differential input amp will be the best for good CMRR. You may not HAVE to do this, you could ground the secondary and then drive our input stage in the DSP. It would need to be cap coupled. However, read these articles and see what would be best for your application. 

    Scientific Conversion, Inc. - Transformers and Inductors (scientificonversion.com)

    Dave T

Children