Hello,
I'm looking for a simple solution to convert microphone audio to S/PDIF stream.
Does Analog Device have products in its portfolio to achieve this functionality?
Thanks.
Pavel.
ADAU1452
Production
The ADAU1452 / ADAU1451 / ADAU1450 are automotive qualified audio processors that far exceed the digital signal processing capabilities of earlier SigmaDSP...
Datasheet
ADAU1452 on Analog.com
ADAU1442
Production
The ADAU1442 / ADAU1445 / ADAU1446 are enhanced audio processors that allow full flexibility in routing all input and output signals. The SigmaDSP® core...
Datasheet
ADAU1442 on Analog.com
Hello,
I'm looking for a simple solution to convert microphone audio to S/PDIF stream.
Does Analog Device have products in its portfolio to achieve this functionality?
Thanks.
Pavel.
Hello Pave147,
Yes, a couple of products.
The ADAU1452 has an SPDIF input and output. The microphone can directly interface with the DSP if it is a digital mic. If it is an analog mic then you will need some sort of codec to be a mic preamp and ADC.
The older ADAU1442 also has an SPDIF interface but it is an older part so I would not use it if possible.
Sample rate will be important. The ADAU1452 can go up to 96kHz fs and if you need to go up to 192kHz fs then you will need to use the ADAU1467/66/63/62 family.
Dave T