ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
AD1938
Production
The AD1938 is a high performance, single-chip codec that provides four analog-to-digital converters (ADCs) with input and eight digital-to-analog converters...
Datasheet
AD1938 on Analog.com
Hi,
Currently I am trying to integrate ESP32 bluetooth I2S output with ADAU1701. My board is based on EVAL-ADAU1701MINIZ-8 design. AUX inputs work fine. If I connect ESP32 with in-built DAC via AUX in, it still works with little noise. However, issue is when I am trying to use the I2S. I am connecting output from ESP32 to following:
1. LRCK - MP4
2. BCLK - MP5
3. SDATA - MP1
Result is only noise. I have been trying to change PLL jumpers, but no luck. Changes resister settings e.g enabling/disabling master mode, changing word length etc. However, all these setting are for SDATA OUT, and I am at this point not much bothered with it as I am using DAC to output to AMP.
Is there anything that I am missing? Do I have to change any clock/frequency settings somewhere?
Thank you in advance.
-Mayuresh
Hi,
In order for better understanding of the issue, I am attaching some screenshot containing
1. signal on sdata
2. Lrck
3. Bclk
Also, incoming signal in SigmaStudio along with the test program and resister setting etc. Hope this would help.
Regards
-Mayuresh
Hi,
In order for better understanding of the issue, I am attaching some screenshot containing
1. signal on sdata
2. Lrck
3. Bclk
Also, incoming signal in SigmaStudio along with the test program and resister setting etc. Hope this would help.
Regards
-Mayuresh