Post Go back to editing

Is it normal to have 0.2% THD with AD1866 at 1kHz and -1 dBFS in a NOS architecture?

Category: Hardware
Product Number: AD1866

Greetings,

I'm testing a setup based on the AD1866 without oversampling and digital filtering, the reconstruction filter is based on the design presented in the datasheet, but I'm using a 4562 instead of a NJM2100.

The THD+N measured using MATLAB and the PC sound card is 0.2%, is this value normal?

The input signal is fed from an Arduino Due based board and the samples are stored in an SD card in PCM WAVE format at 48kHz/16bit.

Best Regards,

Daniel Almeida

Edit Notes

Moved & added tag
[edited by: emassa at 2:40 PM (GMT -5) on 30 Jan 2023]

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.