Hello,
I'm currently considering Adau1467 for an industrial project but I can not achieve I2S_slave output configuration with the ADA1467Z board.
I have an external MCU generating I2S clock as follow :
BCLK : 512kHz ----------> connected to BCLKOUT_0
LRCLK :16kHz -----------> connected to LRCLK_OUT0
Then I try to generate simple SIN WAVE with ADA1467 and send it to SDATA0 AS A I2S :
When BLCK is in master_Mode, it works great. I can see I2S signal on SDATA_OUT0 pin.
When I put BLCK and LRCK in slave_MODE , I have no signal on SDATA_OUT0 pin.
I think I am missing something but I can't get it.
My configuration for slave_MODE is :
Can you help me getting ADA1467 output working in slave_mode ? Also, what does Slave_domain 0 / 1 / 2 / 3 refers to ?
Thank you very much for your time and work.
William