Post Go back to editing

About ADAU1979 signal quality

Category: Hardware

there had a Interference signal approaching 5K

the adau1979 reg cfg in next ( TDM8 + 48K + 12.288MKZ + LRCLK MODE):

addr: 0x0 data : 0x1
addr: 0x1 data : 0xd1
addr: 0x2 data : 0x4a
addr: 0x3 data : 0x7d
addr: 0x4 data : 0x3f
addr: 0x5 data : 0x5a
addr: 0x6 data : 0x0
addr: 0x7 data : 0x10
addr: 0x8 data : 0x32
addr: 0x9 data : 0xf0
addr: 0xa data : 0xa0
addr: 0xb data : 0xa0
addr: 0xc data : 0xa0
addr: 0xd data : 0xa0
addr: 0xe data : 0x2
addr: 0xf data : 0xff
addr: 0x10 data : 0xf
addr: 0x11 data : 0x0
addr: 0x12 data : 0x0
addr: 0x13 data : 0x0
addr: 0x14 data : 0x0
addr: 0x15 data : 0x20
addr: 0x16 data : 0x0
addr: 0x17 data : 0x0
addr: 0x18 data : 0x27
addr: 0x19 data : 0x0
addr: 0x1a data : 0x0

Is it caused by hardware?

  • Hello hebing,

    How are you measuring this? The units are cutoff in your screenshot but it looks like Vrms? So therefore you are going through a DAC and other circuitry?

    The spike is at a curious frequency in that it is not a harmonic of 1kHz. 

    What is the input level to the ADC? At the pins. 

    If you look at figure 6 and 7 in the datasheet, you will see what is expected of the part. This was measured directly digitally. Figure 6 is with a lower level signal and figure 7 is with a -1dBFS signal which is just before clipping. You will see the resulting distortion products are all harmonics of the 1kHz fundamental. 

    So I suspect it is something else in your system that is involved here. 

    I do not think this will be a clock jitter issue but I cannot rule that out. 

    I would look at power and ground carefully. Is there anything in your system that might produce a 4.5kHz signal? LED controllers? 

    Change the input frequency and see if it changes with it?

    Try a level that is about -20dB from full scale. 

    Dave T

  • Hello Dave:

    I‘m very gland for your reply!I had found the reason,the power of ADC not reach expect 8V

    tksy very much.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.