Hi All,
I got some questions about getting start EVAL-ADAU1860.
I've tried to execute the step the document wrote in Lark SDK v3.0.2, but I don't have any example code for Hifi3z and configure for the Xtensa IDE.
The document in Lark SDK v3.0.2 said: You should receive a installment for core release from ADI. Install it to get the LARK support libraries and source
files.
Is that mean I should get the example by buying a set of EVAL-ADAU1860?
My manager tried to buy one EVAL-ADAU1860 but receive that there is shortage in stock.
So my manager tried to borrow one (with only EVAL-ADAU1860EBZ evaluation board).
With only the board on hand.
1. Do I need mIDAS-Link emulator to debug on the Hifi3z DSP or are there any others JTAG I can use for uploading the code and debugging?
2. Is there any sample code and SDK for audio recording on Hifi3z DSP for EVAL-ADAU1860?
Thanks.
Hi Liao
J-link also can be used to connect to Hifi3z DSP core.
Hi JakubJ,
Thanks for your reply.
Yes, you are right, Jlink V8 or newer version can be supported.
Hi Liao,
SDK can be downloaded in webpage - 'Software & Systems Requirements', ADAU1860 Datasheet and Product Info | Analog Devices
As for example code, detailed info haven't be published on official web page. Currently, it's necessary to ask support from local sales or FAE if relative resources needed.
Thanks.
Diane
Dear JakubJ & DianeLi,
Thanks for the reply.
I got the local FAE support and get the example.
The only problems now is the board didn't work as it should be.
Dear JakubJ & DianeLi,
Thanks for the reply.
I got the local FAE support and get the example.
The only problems now is the board didn't work as it should be.