Post Go back to editing

Audio example for EVAL-ADAU1860 Hifi3z DSP

Thread Summary

The user inquired about getting started with EVAL-ADAU1860, specifically regarding the need for a mIDAS-Link emulator for debugging and the availability of sample code. The final answer confirmed that J-link V8 or newer can be used instead of mIDAS-Link, and that the SDK can be downloaded from the ADAU1860 product page. The user also noted that they obtained example code from local FAE support, but the board is not functioning as expected.
AI Generated Content

Hi All,

I got some questions about getting start EVAL-ADAU1860.

I've tried to execute the step the document wrote in Lark SDK v3.0.2, but I don't have any example code for Hifi3z and configure for the Xtensa IDE.
The document in Lark SDK v3.0.2 said: You should receive a installment for core release from ADI. Install it to get the LARK support libraries and source
files.

Is that mean I should get the example by buying a set of EVAL-ADAU1860?

My manager tried to buy one EVAL-ADAU1860 but receive that there is shortage in stock.
So my manager tried to borrow one (with only EVAL-ADAU1860EBZ evaluation board).

With only the board on hand.

1. Do I need mIDAS-Link emulator to debug on the Hifi3z DSP or are there any others JTAG I can use for uploading the code and debugging?

2. Is there any sample code and SDK for audio recording on Hifi3z DSP for EVAL-ADAU1860?

Thanks.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.