Post Go back to editing

About the analog input rating of ADAU1979

Hello

I have a question about the ADAU1979 analog input terminal ratings.
The Analog Input Voltage (Signal Pins) is specified as -0.3V to 3.6V in the "ABSOLUTE MAXIMUM RATINGS" section on page 7 of the data sheet.


However, ADAU1979 is differentially compatible with 4.5Vrms.
At the differential 4.5Vrms input, I think each AIN pin has 2.25Vrms input.
In this case, it will be 6.36Vp-p, and I think that it will exceed the rated value of the analog input.

Can I use the differential 4.5Vrms input without any problems?

I would be grateful if you could reply.

Best Regards,
Knj

Parents Reply Children
No Data