Post Go back to editing

ADAU1361 ADC Full-Scale Level with negative PGA gain

Hello Analog Community,

The ADAU1361 datasheet states an ADC full-scale level of 1 Volts rms when operated with AVDD = 3.3 Volts. My question is, when using the PGA in single ended mode (line-in) with a gain of -6 dB, will the device accept 2 Volts rms without clipping?

Thanks and Best Regards!
Ulrich



corrected spelling errors
[edited by: AudioDeCologne at 11:03 PM (GMT -5) on 17 Dec 2020]