Post Go back to editing

Choosing a good opamp for a mic preamp

I'm looking for recommendations for a good opeamp to use in a simple microphone preamp circuit for ADI's MEMS microphones. The noise floor of these microphones is at -100 dBV (10 uV), A-weighted, with a 20 kHz bandwidth. The typical use of this preamp will apply between about 12-36 dB of gain, depending on the application. An example of a typical implementation of this non-inverting circuit is shown in Figure 8 of the ADMP404 datasheet.

Of course, the AD797 is a great audio opamp, but this may be overkill for some applications. I have used the OP275 and AD8606 in audio designs, but I've been looking at other opamps as well. The noise, distortion, and slew rate specs of the AD8597, ADA4841 (replacement for the OP275?), and ADA4075 (recommended in this thread) look good. Are there any good choices I'm missing here, or other specs I should be thinking of?

The MEMS microphone datasheets currently show an OP177 in a preamp circuit. Is this a good choice, or would another device be better as a general, standard recommendation?

  • Thank you for the suggestions. I should've mentioned something about the supplies in my original post; that certainly affects which device we would select. The MEMS microphones work with a 1.5-3.6 V supply. For many designs using these microphones, the only available supply may be 1.8 or 3.3 V. Which opamps would you suggest to use at these lower voltages?

    The MEMS mics have a lower -3 dB corner at 100 Hz, so I'd want to have a decent response down to that frequency.

    This isn't for a specific design right now. I'm making sure that our recommendations in the datasheet are up-to-date, and that I'm ready to answer the question when it's inevitably asked of me!

  • I certainly understand that 1.8 V may be a bit too low for a good preamp. I don't think it's unreasonable to think that many or most designs with an analog preamp circuit will have at least 3.3 V available. Thank you again for the suggestions. I think there's a good selection of different parts mentioned here that could be used for this application.

  • Hi Jerad,

    I would recommend the ADA4841-1, -2 (single and dual version) in the low voltage application that you are discussing; it is spec'd down to 2.7 V. The ADA4841 has half the Input Noise (2.1 nV/rtHz) and is lower power than the other parts that have been discussed. Unfortunately, it is a little more expensive.

    BR,

    ColemanR

  • Hi Coleman,

    Thanks for the additional suggestion. The ADA4841 looks like it could be a good choice for low-noise, low-power applications that may be a bit less sensitive to cost.

  • I want to update this older thread now that we have a new application note on exactly this topic. AN-1165: Op Amps for MEMS Microphone Preamp Circuits has recently been published and is available to download. This app note covers some of the key op amp specifications to consider in a preamp design, shows a few basic circuits, and provides a table of Analog Devices, Inc., op amps that may be appropriate for a preamp design.

    Thanks to everyone to answered questions in this thread and others (like here and here). These replies were all very useful as I put together this app note.