How can I determine what is the peak output voltage from an analog MEMS microphone? Some data sheets only show the peak sound pressure level (SPL). I need to know the voltage at that SPL to ensure that the microphone doesn't clip my preamp circuit.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADMP401
Obsolete
Analog Devices has sold its MEMS Microphone product line to InvenSense.
Please visit the InvenSense ADMP401 product page for all technical support and...
ADMP401 on Analog.com
ADMP504
Obsolete
Analog Devices has sold its MEMS Microphone product line to InvenSense.
Please visit the InvenSense ADMP504 product page for all technical support and...
ADMP504 on Analog.com
ADMP404
Obsolete
Analog Devices has sold its MEMS Microphone product line to InvenSense.
Please visit the InvenSense ADMP404 product page for all technical support and...
ADMP404 on Analog.com
ADMP405
Obsolete
Analog Devices has sold its MEMS Microphone product line to InvenSense.
Please visit the InvenSense ADMP405 product page for all technical support and...
ADMP405 on Analog.com
How can I determine what is the peak output voltage from an analog MEMS microphone? Some data sheets only show the peak sound pressure level (SPL). I need to know the voltage at that SPL to ensure that the microphone doesn't clip my preamp circuit.
An analog microphone's peak output voltage can be derived from the sensitivity and maximum SPL specs. Let's use the ADMP404, which has a -38 dBV sensitivity and 120 dB SPL maximum acoustic input, as an example.
The -38 dBV sensitivity means that the ADMP404 will have a 12.5 mV rms output for a 94 dB SPL (1 Pascal) acoustic input. This is calculated using the equation 10^(-38 dBV/20) = rms voltage output. Note that both this voltage output and acoustic input are given as rms units. In peak levels, the microphone will output a 17.8 mV peak signal with a 97 dB SPL (peak) input. This voltage is equivalent to -35 dBV, which is naturally 3 dB higher than the sensitivity spec which is given for rms signals.
The maximum (peak) acoustic input that the microphone can input before clipping is 120 dB SPL, which is 23 dB above the reference sensitivity level (97 dB SPL peak) that is described above. To get the peak voltage at this SPL you can just add 23 dB to the -35 dBV level to get a -12 dBV level at the maximum acoustic input. This can be converted to a peak voltage by peak output voltage = 10^(-12 dBV/20), or about 250 mV peak. Double this to get the peak-to-peak output voltage, which will be about 500 mV. Now you can use this signal level to design your system's gain staging so that you have sufficient headroom and can avoid clipping the microphone output.
You can use the equations above for different microphones with different sensitivities and maximum acoustic inputs to calculate their peak output voltages. Newer MEMS microphone data sheets, such as the one for the ADMP504, include the maximum output voltage in the specifications table.
Answered and Closed