Post Go back to editing

ADMP421 bias in output signal.

I am working with the ADMP421 MEMS microphone and the ADAU1761. I am also using the ADAU1761 as a codec for an extenal microphone. When the system is configured for the external microphone, there is a zero bias on the output and the high frequency content of the sound is easily picked up. However, when I configure the system for the ADMP421 microphone, I am seeing a very large positive bias on the output, (~15% of the output range). Also, I am not hearing much of the high frequency content of the sound. Is there a setting in SigmaStudio that could be causing this? My company had some problems with the original pad layout suggested for the ADMP421. Could this be a factor in producing the bias I am seeing?

Parents
  • One more point that I forgot to mention in my last post...I did confirm that the ADAU1761's high pass filter is implemented digitally, so it will work for both analog inputs and digital microphones. The latest test you described above already indicates this, but I just wanted to post it here explicitly (either for you or whoever might read this thread in the future).

Reply
  • One more point that I forgot to mention in my last post...I did confirm that the ADAU1761's high pass filter is implemented digitally, so it will work for both analog inputs and digital microphones. The latest test you described above already indicates this, but I just wanted to post it here explicitly (either for you or whoever might read this thread in the future).

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.