Post Go back to editing

ADMP421 bias in output signal.

I am working with the ADMP421 MEMS microphone and the ADAU1761. I am also using the ADAU1761 as a codec for an extenal microphone. When the system is configured for the external microphone, there is a zero bias on the output and the high frequency content of the sound is easily picked up. However, when I configure the system for the ADMP421 microphone, I am seeing a very large positive bias on the output, (~15% of the output range). Also, I am not hearing much of the high frequency content of the sound. Is there a setting in SigmaStudio that could be causing this? My company had some problems with the original pad layout suggested for the ADMP421. Could this be a factor in producing the bias I am seeing?

Parents
  • Hi Jerad,

    After some more trouble shooting, I've found out a few more things and I was wondering if this might be what is causing this issue. Although my system is using only the one ADMP421 microphone, when I spy on the I2S bus, I am seeing samples on both channels that have to be coming from the same source. I have an idea that our problems with the microphone pcb layout may have caused the microphone to output samples on both channels but what happens when it is forced to output samples at twice the rate the clock is set for? Does the microphone need the half cycle of the I2S frame clock it is not transmitting to properly acquire the sample? I get the impression I have inadvertently created a low pass filter in the signal chain.

Reply
  • Hi Jerad,

    After some more trouble shooting, I've found out a few more things and I was wondering if this might be what is causing this issue. Although my system is using only the one ADMP421 microphone, when I spy on the I2S bus, I am seeing samples on both channels that have to be coming from the same source. I have an idea that our problems with the microphone pcb layout may have caused the microphone to output samples on both channels but what happens when it is forced to output samples at twice the rate the clock is set for? Does the microphone need the half cycle of the I2S frame clock it is not transmitting to properly acquire the sample? I get the impression I have inadvertently created a low pass filter in the signal chain.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.