Post Go back to editing

AD1939 - Clocks questions

Hello,

I'am using an AD1939 codec and I have a crystal on my board which generates 12,288 MHz (256 x Fs in my case, since I'll use only 48 kHz as a sample rate) and this crystal is connected to the MCLKI/XI pin of the AD1939.

All the systems is connected to a FPGA, which will receive the 12,288 MHz as well.

In my registers, I am going to put the MCLKI/XI for the PLL input in PLL and Clock Control register 0.

Here are my questions :

For the PLL and Clock control register 1, what is exactly the difference between PLL Clock and MCLK for the DAC and ADC source ?

The PLL isn't supposed to generate the MCLK ? In my case, putting both in PLL Clock would be OK ?

About the LRCLK, what is the difference between Slave and Master ? Do I have to provide a 48 kHz signal in master mode or is it self-generated from my MCLK since I provide it with the MCLKI/XI ?

If I have to generate a 48 kHz signal, do you think that generating it from the FPGA would be OK or it would jitter the signal so badly it wouln't be usable ?

About the BCLK, I'm planning to put in Master mode and to put in Internally Generated. If I get it right, it will be generated and I don't have to connect anything on the BCLK ?

They are maybe "silly" questions, and I apologize, I'm new in design creation :-)

Thanks in advance,

Florent

Parents
  • Hi Florent,

    The crystal circuit in the IC requires the loop to be closed in order to ring at the specified frequency. Please consult the User Guide for the EVAL-AD1939AZ for the circuit.

    Maybe you are using an active oscillator? In that case, there is no need to connect the MCLKO pin to anything.

    Best regards,

    Coleman

Reply
  • Hi Florent,

    The crystal circuit in the IC requires the loop to be closed in order to ring at the specified frequency. Please consult the User Guide for the EVAL-AD1939AZ for the circuit.

    Maybe you are using an active oscillator? In that case, there is no need to connect the MCLKO pin to anything.

    Best regards,

    Coleman

Children
No Data