Post Go back to editing

Conditioning ADMP404 output for ADC

I am looking into using the ADMP404 MEMS mic as a source for medium quality (100-3,000Hz) voice.  Everything runs off a low power 3v supply.  I need to compress/condition the audio input and also amplify it so that it can be digitized using a 12 bit ADC at 8 Ksps.  Being cost sensitive, I would like to use the minimum number of components.

I am designing for normal operation at 60 to 80 dB-SPL, so with the ADMP404 (-38 dBV sensitivity) I would need a gain of between 72 to 52 dB (4000 to 400).  Prototyping will help select the final gain.

The SSM2167 seems very attractive, but it does not have sufficient gain to swing an ADC.  The SSM2166 is not quite suitable.  Is there a single chip alternative that avoids having a compressor plus op-amp configuration?  If I had to use an op amp, would the AD8542 or AD8506 be appropriate?  I have read (and appreciated) the AN-1165 and AN-1112 design notes.

I am also looking into noise cancelling but could not find any design notes.  I was thinking of two ADMP404, one on each side of the PCB.  Can you suggest any designs or guidelines?

thanks

--raj

Message was edited by: Rajaram Pejaver (oops, cut & paste error with mic name)

Parents
  • Hi Raj,

    Am I correct that you're looking to add 52 dB of gain to the microphone's output so that an 80 dB SPL signal is amplified to 0 dBV (1 Vrms)? Even if you're only intending to capture voice in the typical speech range (60-80 dB SPL), I don't think that you'll want to amplify the signal so that all inputs above 80 dB SPL will be clipped. Even for speech signals with an rms level of 60-80 dB SPL, they may have a crest factor (difference between the rms level and peak level) of 20 dB. This would mean that the peaks of the speech signal could reach 80-100 dB SPL. If you still want to match the peaks of the acoustic signal to 0 dBV, then you'll just need 32 dB of gain. On top of that, if you assume that someone using your design may speak right into the microphone, the input signal could be at an even higher SPL. You may want to configure your design to account for that by using even less gain.

    It does look like the SSM2167 would be a good device to pair with the ADMP404. We have a Circuit from the Lab describing exactly this setup (CN-0262). In a voice capture application, the compression and noise gating that the SSM2167 offers may make your captured sound more intelligible by reducing the dynamic range while still applying a reasonable gain. If you just want to use an op amp in a straight amplification circuit, then either the AD8542 or AD8506 should work fine.

    Could you explain more about what exactly you're looking for with "noise cancelling"? Are you trying to do acoustic noise cancellation, or are you just looking for a "noise cancelling" microphone with a figure-8 pickup pattern?

Reply
  • Hi Raj,

    Am I correct that you're looking to add 52 dB of gain to the microphone's output so that an 80 dB SPL signal is amplified to 0 dBV (1 Vrms)? Even if you're only intending to capture voice in the typical speech range (60-80 dB SPL), I don't think that you'll want to amplify the signal so that all inputs above 80 dB SPL will be clipped. Even for speech signals with an rms level of 60-80 dB SPL, they may have a crest factor (difference between the rms level and peak level) of 20 dB. This would mean that the peaks of the speech signal could reach 80-100 dB SPL. If you still want to match the peaks of the acoustic signal to 0 dBV, then you'll just need 32 dB of gain. On top of that, if you assume that someone using your design may speak right into the microphone, the input signal could be at an even higher SPL. You may want to configure your design to account for that by using even less gain.

    It does look like the SSM2167 would be a good device to pair with the ADMP404. We have a Circuit from the Lab describing exactly this setup (CN-0262). In a voice capture application, the compression and noise gating that the SSM2167 offers may make your captured sound more intelligible by reducing the dynamic range while still applying a reasonable gain. If you just want to use an op amp in a straight amplification circuit, then either the AD8542 or AD8506 should work fine.

    Could you explain more about what exactly you're looking for with "noise cancelling"? Are you trying to do acoustic noise cancellation, or are you just looking for a "noise cancelling" microphone with a figure-8 pickup pattern?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.