Post Go back to editing

Conditioning ADMP404 output for ADC

I am looking into using the ADMP404 MEMS mic as a source for medium quality (100-3,000Hz) voice.  Everything runs off a low power 3v supply.  I need to compress/condition the audio input and also amplify it so that it can be digitized using a 12 bit ADC at 8 Ksps.  Being cost sensitive, I would like to use the minimum number of components.

I am designing for normal operation at 60 to 80 dB-SPL, so with the ADMP404 (-38 dBV sensitivity) I would need a gain of between 72 to 52 dB (4000 to 400).  Prototyping will help select the final gain.

The SSM2167 seems very attractive, but it does not have sufficient gain to swing an ADC.  The SSM2166 is not quite suitable.  Is there a single chip alternative that avoids having a compressor plus op-amp configuration?  If I had to use an op amp, would the AD8542 or AD8506 be appropriate?  I have read (and appreciated) the AN-1165 and AN-1112 design notes.

I am also looking into noise cancelling but could not find any design notes.  I was thinking of two ADMP404, one on each side of the PCB.  Can you suggest any designs or guidelines?

thanks

--raj

Message was edited by: Rajaram Pejaver (oops, cut & paste error with mic name)

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.