Hi,
When external clock signal is supplied to MCLK_I pin of AD1895/96, how much jitter is acceptable for proper operation?
AD1895
Production
The AD1895 is a 24-bit, high-performance, single-chip, second-generation asynchronous sample rate converter. Based upon Analog Devices experience with...
Datasheet
AD1895 on Analog.com
AD1896
Production
The AD1896 is a sample rate converter; it is second generation and 24-bit, high-performance, single-chip, and asynchronous. Based upon Analog Devices experience...
Datasheet
AD1896 on Analog.com
Hi,
When external clock signal is supplied to MCLK_I pin of AD1895/96, how much jitter is acceptable for proper operation?
Hi,
Unfortunately, we do not have any characterization data to show the outside range of operation of the AD1895/96 as a function of increasing jitter on MCLK. There is an internal circuit that reduces the jitter from the MCLK input to the BCLK and LRCLK generated by the AD1895/96, but at some point it will stop being effective and the clocks in the part will exhibit a reduced version of the jitter as well.
Best regards,
Coleman