Post Go back to editing

Adi Evaluation board CN0284 beamforming processing need algorithm?

hi adi :

I bought a evaluation board cn0284 (http://www.analog.com/zh/circuits-from-the-lab/cn0284/vc.html)from adi ,now I have some question,In the adi's application vedio: http://videos.analog.com/video/1979997938001/Microphone-Array-Beamforming-with-the-ADMP504/

said the beamforming processing need the beamforming processing algorithm support,but I view the Schematic of cn0284,I don't clear

whether  the cn0284 board need beamforming processing algorithm support?

Parents
  • The circuit shown in CN0284 is performing the beamforming processing, but is doing this with analog circuits, rather than on a DSP. The video that you've linked to above is doing similar processing, but that is being done on a SigmaDSP. The analog beamforming in CN0284 is done with allpass filters (delay) and summing amplifiers (subtraction). With the two microphone boards connected to the power & processing board, this design is set up to do microphone array beamforming.

Reply
  • The circuit shown in CN0284 is performing the beamforming processing, but is doing this with analog circuits, rather than on a DSP. The video that you've linked to above is doing similar processing, but that is being done on a SigmaDSP. The analog beamforming in CN0284 is done with allpass filters (delay) and summing amplifiers (subtraction). With the two microphone boards connected to the power & processing board, this design is set up to do microphone array beamforming.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.