In our applications we have observed that SSM2166 is vulnerable/susceptible to Radio Emissions (with AM modulation) from near by VHF system. In order to overcome this pls suggest the alternative for SSM2166.....
SSM2166
Production
The SSM2166 integrates a complete and flexible solution for conditioning microphone inputs in computer audio systems. It is also excellent for improving...
Datasheet
SSM2166 on Analog.com
In our applications we have observed that SSM2166 is vulnerable/susceptible to Radio Emissions (with AM modulation) from near by VHF system. In order to overcome this pls suggest the alternative for SSM2166.....
Hi,
Thank you, Bob! The suggestion of an LC on the front end is excellent.
I would add that the SSM2166 can be treated as a differential input. Is your source differential? Are you using a twisted pair…
hi KJ Bob & Coleman,
Sorry for the delay. It was long time i had opened engineer forum. My system is differential and today i made one filter circuit with series 47uH and shunt 0.01uF. Two circuits…
Could you share the schematic for the MIC-HI and MIC-LO inputs through to the SSM? Are these two inputs going to opposite sides of the primary, are they using normalling jacks, etc? How is the ground scheme…
Could you share the schematic for the MIC-HI and MIC-LO inputs through to the SSM? Are these two inputs going to opposite sides of the primary, are they using normalling jacks, etc? How is the ground scheme implemented?
Could you share the schematic for the MIC-HI and MIC-LO inputs through to the SSM? Are these two inputs going to opposite sides of the primary, are they using normalling jacks, etc? How is the ground scheme implemented?