Post Go back to editing

i am looking for suitable replacement for SSM2166 (mic preamp)...pls suggest the best solution

In our applications we have observed that SSM2166 is vulnerable/susceptible to Radio Emissions (with AM modulation) from near by VHF system. In order to overcome this pls suggest the alternative for SSM2166.....

Parents
  • Dear Mr.Bob,

     

    Mr.Bob, thanks for ur reply and showing interest in this problem.

     

    Here in our system the MIC-HI & MIC-LO lines are given to a transformer which is a centre tapped one. And the secondary of the transformer is connected to Pin.no.7 (IN+) of SSM2166. And other end of secondary of the transformer is connected to pin no.6 (IN-) through Resistor and capacitor.

     

    So, i will try to connect 220pF in b/w pin no. 6 & 7. It is an VHF AM transceiver antenna is near by to the audio system. And our audio system is in a sheilded box only. Pls suggest any material comes which can be pasted inside the audio system box to eliminate the RF entering into audio system.

     

    Or any other differential amplifier will u suggest beofre the micrphone signals enters into the Audio system. In our audio system SSM2166 is the front end stage.

     

     

    Thanks & Regards,

    Naveen S

     

Reply
  • Dear Mr.Bob,

     

    Mr.Bob, thanks for ur reply and showing interest in this problem.

     

    Here in our system the MIC-HI & MIC-LO lines are given to a transformer which is a centre tapped one. And the secondary of the transformer is connected to Pin.no.7 (IN+) of SSM2166. And other end of secondary of the transformer is connected to pin no.6 (IN-) through Resistor and capacitor.

     

    So, i will try to connect 220pF in b/w pin no. 6 & 7. It is an VHF AM transceiver antenna is near by to the audio system. And our audio system is in a sheilded box only. Pls suggest any material comes which can be pasted inside the audio system box to eliminate the RF entering into audio system.

     

    Or any other differential amplifier will u suggest beofre the micrphone signals enters into the Audio system. In our audio system SSM2166 is the front end stage.

     

     

    Thanks & Regards,

    Naveen S

     

Children
No Data