Post Go back to editing

i am looking for suitable replacement for SSM2166 (mic preamp)...pls suggest the best solution

In our applications we have observed that SSM2166 is vulnerable/susceptible to Radio Emissions (with AM modulation) from near by VHF system. In order to overcome this pls suggest the alternative for SSM2166.....

Parents
  • Hi,

    Thank you, Bob! The suggestion of an LC on the front end is excellent.

    I would add that the SSM2166 can be treated as a differential input. Is your source differential? Are you using a twisted pair wire with a grounded shield, to connect your source with the SSM2166? Even a single-ended source can be improved by treating it as much like a differential source as possible. Can you share some more information about your system?

    Best regards,

    Coleman

Reply
  • Hi,

    Thank you, Bob! The suggestion of an LC on the front end is excellent.

    I would add that the SSM2166 can be treated as a differential input. Is your source differential? Are you using a twisted pair wire with a grounded shield, to connect your source with the SSM2166? Even a single-ended source can be improved by treating it as much like a differential source as possible. Can you share some more information about your system?

    Best regards,

    Coleman

Children
No Data