Post Go back to editing

SSM2142 Balanced Line Driver breaking input impedance

Hi all,

my problem concerns the breaking of the input stage of the chip SSM2142 which occurs some time during a test cycle.

My testbench is attached for information.

How can see, the SSM2142 is connected to the "secondary" windings of a LVDT excited with a 5Vrms/10kHz sine wave on the "primary" windings by means of the SSM2143 differential line driver connected to an arbitray waveforms generator. An oscilloscope is connected to the differential output of the SSM2142 Line Driver.

After about 2hours of test I see that the signal at the output of the SSM2142 is reduced by 1\2. Measuring with a multimeter the resistance at the input of SSM2142 I found that the value was lowered to about 92.76ohm. In normal condition I measure a resistance of about 50kohm.

Do you have idea why this could happen?

What is it the possible root cause of the input resistance "breaking" of the SSM2142'buffer stage of the cross-coupled topology?

Note: The "Test Board" is "hot inserted" in the test bench (i.e. the power supply and the signal generator are "ON" and "fully operational").

Best Regards

Francesco Carbone

Parents
  • Hello Francesco,

    Well, that was just a guess on my part that there may be a short to one of the power rails. To find the "root" cause will require a lot more investigation, information and time. We would need a faulty part to do some failure analysis to see what was over-stressed to give us an idea of where to look at your design. Then we would need your schematics and PCB layout information and more details on the input signals to your board. This is all an expensive and time consuming undertaking. Since this part is quite mature and has been in production for some time I doubt there is a problem with the part. So that is why I suggested to look closely at the input pin protection circuits on your board. This is based on a "most likely" cause based on the info you have supplied so far.

    Feel free to send me a private message or an email and we can discuss this in more detail.

    Thanks,

    Dave T

Reply
  • Hello Francesco,

    Well, that was just a guess on my part that there may be a short to one of the power rails. To find the "root" cause will require a lot more investigation, information and time. We would need a faulty part to do some failure analysis to see what was over-stressed to give us an idea of where to look at your design. Then we would need your schematics and PCB layout information and more details on the input signals to your board. This is all an expensive and time consuming undertaking. Since this part is quite mature and has been in production for some time I doubt there is a problem with the part. So that is why I suggested to look closely at the input pin protection circuits on your board. This is based on a "most likely" cause based on the info you have supplied so far.

    Feel free to send me a private message or an email and we can discuss this in more detail.

    Thanks,

    Dave T

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.