Post Go back to editing

SSM2142 Balanced Line Driver breaking input impedance

Hi all,

my problem concerns the breaking of the input stage of the chip SSM2142 which occurs some time during a test cycle.

My testbench is attached for information.

How can see, the SSM2142 is connected to the "secondary" windings of a LVDT excited with a 5Vrms/10kHz sine wave on the "primary" windings by means of the SSM2143 differential line driver connected to an arbitray waveforms generator. An oscilloscope is connected to the differential output of the SSM2142 Line Driver.

After about 2hours of test I see that the signal at the output of the SSM2142 is reduced by 1\2. Measuring with a multimeter the resistance at the input of SSM2142 I found that the value was lowered to about 92.76ohm. In normal condition I measure a resistance of about 50kohm.

Do you have idea why this could happen?

What is it the possible root cause of the input resistance "breaking" of the SSM2142'buffer stage of the cross-coupled topology?

Note: The "Test Board" is "hot inserted" in the test bench (i.e. the power supply and the signal generator are "ON" and "fully operational").

Best Regards

Francesco Carbone

Parents
  • Hi Dave,

    The LVDT transducers is typically a “step-down transformers”…in my application excite the primary with a max differential sine wave of 20Vpp@5kHz and the maximum  LVDT sine wave response is maximum 3Vpp@5kHz (as a function of “the core” material and position of the inserted in the LVDT).

    About the maximum input voltage range of SSM2142 balanced line driver, Does the Vin =+-7.071V is the maximum input voltage that provide the clip level output voltage of 10.5Vrms? Is it correct? Does the maximum input voltage equal to the power supply of SSM2142?

    The failure is permanent. The devices no longer works after a power-off\power-on of the power supply.

    About the input impedance of SSM2142, I’ve measured the “static” impedance with the board without power supply applied with a digital multi-meter in ohm configuration. Probably the input impedance of 10k typical provided in the datasheet refer to a “dynamic” impedance providing the power supply to the device.  The “static” impedance measurement in my application is useful to detect static failure in the board as short\open condition.

    Do you have others suggestion on what’s could be the “root” cause of this failure?

    Do you have a failure analysis of SSM2142?

    Thanks for the support.

    Best Regards.

    Francesco C.

Reply
  • Hi Dave,

    The LVDT transducers is typically a “step-down transformers”…in my application excite the primary with a max differential sine wave of 20Vpp@5kHz and the maximum  LVDT sine wave response is maximum 3Vpp@5kHz (as a function of “the core” material and position of the inserted in the LVDT).

    About the maximum input voltage range of SSM2142 balanced line driver, Does the Vin =+-7.071V is the maximum input voltage that provide the clip level output voltage of 10.5Vrms? Is it correct? Does the maximum input voltage equal to the power supply of SSM2142?

    The failure is permanent. The devices no longer works after a power-off\power-on of the power supply.

    About the input impedance of SSM2142, I’ve measured the “static” impedance with the board without power supply applied with a digital multi-meter in ohm configuration. Probably the input impedance of 10k typical provided in the datasheet refer to a “dynamic” impedance providing the power supply to the device.  The “static” impedance measurement in my application is useful to detect static failure in the board as short\open condition.

    Do you have others suggestion on what’s could be the “root” cause of this failure?

    Do you have a failure analysis of SSM2142?

    Thanks for the support.

    Best Regards.

    Francesco C.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.