Post Go back to editing

ADAU1701 CLOCK DRIVER

Thread Summary

The user inquired about using a DS1080CL clock generator to drive 8 ADAU1701 DSPs over 18 inches of trace. The support engineer advised against it due to the DS1080CL's limited output drive capability and recommended using a 12.288 MHz packaged oscillator buffered with a 74LVC2G34, including a 50 ohm series resistor to reduce ringing. The circuit successfully drives up to six ADAU1701s, and pin 31 can be left unconnected. Longer trace lengths and multiple stubs may require individual buffers for each board.
AI Generated Content

I am looking for a clock driver to drive 8 ADAU1701  and was looking @ the one in the link and was not sure if  that circuit was suitable to drive 8 ADAU1701 over a 18 inch length of trace, DS1080CL datasheet, Pinout ,application circuits Spread-

Spectrum Crystal Multiplier

Is there an analog device  ic I can use that is similar to the one in the link  ?

Thanks in advance

Parents Reply Children
No Data