Post Go back to editing

ADAU1772 DC coupling input/outputs

Hello,

i am looking at the ADAU1772 and i was wondering if you could clarify if there are any requirements for the coupling type.  on the evaluation board it shows that all inputs and outputs are AC coupled, however, if the signal is within the allowable range of the ADC (i.e. 2.54Vpp with VDD = 3.3V 0dBFS) can the inputs be DC coupled?

similarly for the outputs can they be DC coupled without impact to the ADAU1772?

Thanks!

  • Hello Rene,

    The simplest and most trouble free way to run the part is to AC couple. Should you want to DC couple then the 2.54 Vpp signal you mentioned has to be centered around the common mode voltage and not ground. Internally, the CM voltage is derived by simply dividing the AVDD by 2. You could do this externally or you can use the CM pin to bias your external circuit around this voltage. Then you will most likely have to cap couple the external circuit as well so you may not gain anything by doing this.

    You cannot draw any current (well, minimal current) from this pin. The source impedance is 5k ohms so if you do use this pin for a reference you will probably want to buffer it with a low noise opamp to provide a low impedance drive. This will help prevent crosstalk and not draw/sink current from the pin.

    Regarding the DAC/HP outputs. The same applies. It will be centered around the CM voltage. In the datasheet there is a section about how to use ground centered headphones and the next section talks about the pre-charge circuit to reduce clicks and pops. So if you are using the output as a line output you will need to cap couple at some point.

    Dave T


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.