about SPI specification on AD1934(DAC) data sheet

Hello all,

I have some questions in AD1934 (DAC) SPI specification.

 

Question

 

In terms of tCOE, tCOH, and tCOTS,

what the figure9 says and what the table 7 says are different.

Could you explain about this?

 

■tCOE

CCLK freqency is 4.1MHz so the 1CCLK period is 240ns.

In my understanding, tCOE in figure 9 is wrong.

tCOE should be between the CLATCH falling and COUT rising.

In the figure there are 14 data(D10-D23).

To sample one data, I need 240ns CCLK so 14 data would require 3.36us(=3360ns).

But the table 7 says that the tCOE max is just 30 ns. I do not understand.

 

■tCOH

Gennerally speaking, I guess CCLK "rising" would sample the data, not falling. Is this is this right information. I am asking this just in case.

 

 

■tCOTS

The figure9 and the table7 are talking different thing.

 

Best Regards,

AD1934_SPI_timing.xlsx
Parents
No Data
Reply Children
No Data