Post Go back to editing

RMS-to-DC for Sound Pressure Level measurement

Hi,

I want to measure the RMS value of a microphone's output voltage (to get the SPL value in dB).

I see a lot of RMS-to-DC IC seem to do that but I am wondering :

At a given moment, if I read the output of the RMS chip (on an ADC), is the RMS (the average/mean part) calculated on the last 10ms ? 100ms ? 1sec ?

In other words, I want to read the RMS value every second. So I want it to be representative of the last second that just passed not the last 10ms.

How is it related to the "settling time" parameter (if it is) ?

Best regards,

V.

Parents
  • Hello Valentin,

    You should post this question in the "Amplifiers" space of the forum. There it will be seen by the proper support people. You should also search EngineerZone for the part number and you will see there are many posts that may answer your question.

    One other thing to consider is using a SigmaDSP for your application. I do not know what else you plan to do before and after the RMS converter but with a SigmaDSP like the ADAU1761 you would get a pre amp, several inputs and DAC outputs along with the DSP. The DSP can be programmed using SigmaStudio making it relatively easy to program an application. We do have cells (blocks) in the library that does RMS conversion. Then you can continue to process the signal in the DSP to do what you need. So have a look and see if it would work for your intended application.

    http://www.analog.com/media/en/technical-documentation/data-sheets/ADAU1761.pdf

    Thanks,

    Dave T

Reply
  • Hello Valentin,

    You should post this question in the "Amplifiers" space of the forum. There it will be seen by the proper support people. You should also search EngineerZone for the part number and you will see there are many posts that may answer your question.

    One other thing to consider is using a SigmaDSP for your application. I do not know what else you plan to do before and after the RMS converter but with a SigmaDSP like the ADAU1761 you would get a pre amp, several inputs and DAC outputs along with the DSP. The DSP can be programmed using SigmaStudio making it relatively easy to program an application. We do have cells (blocks) in the library that does RMS conversion. Then you can continue to process the signal in the DSP to do what you need. So have a look and see if it would work for your intended application.

    http://www.analog.com/media/en/technical-documentation/data-sheets/ADAU1761.pdf

    Thanks,

    Dave T

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.